Cancel
Showing results for 
Search instead for 
Did you mean: 

Complex Bend in NX 9

Experimenter
Experimenter

Hello,

 

I am trying to figure out how to do a complex bend like the one shown below. The images are of a body that was imported. I have to do my own which is slightly different then this one and can not figure out how they did this. Any suggestions would be helpful.

 

Thank you,

 

-MikeBend 1.PNGBend 2.PNGBend 3.PNG

2 REPLIES

Re: Complex Bend in NX 9

Siemens Phenom Siemens Phenom
Siemens Phenom

I suggest using either a Contour Flange or a Lofted Flange.

 

Without the part file in hand, it is hard to make a recommendation.

 

Both methods are shown in the Help Documentation.

Re: Complex Bend in NX 9

Siemens Legend Siemens Legend
Siemens Legend

If you can upload a part file it would be a little easier to understand the problem.