Cancel
Showing results for 
Search instead for 
Did you mean: 

Component overide breaking ignoring fixed contraint of Parent assembly

Master
Master

We have machine assemblies and do component overides on certain components to show the drawings correctly. As we moved into NX 11 when we do a component overide on the child, suppress the assembly constraint that controls the movement we need, and then apply our new constraint it moves the whole machine not the component. The machine is brought in at abs origin and then a fixed constraint is applied. In 8.5 we had some but not much problem with this. Any ideas?

 

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000
3 REPLIES 3

Re: Component overide breaking ignoring fixed contraint of Parent assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

It would help if you could upload some images of the constraints navigator for the level where the override takes place. A before and after picture would be good to show the type of constraints that are being added by the system.

Regards,
Abe

Re: Component overide breaking ignoring fixed contraint of Parent assembly

Master
Master

Ok finally got back to this. Here is a few screenshots of the constraints.

 

Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Component overide breaking ignoring fixed contraint of Parent assembly

Siemens Phenom Siemens Phenom
Siemens Phenom
This is not really enough info to go on.
One thing you can do is check if there is anything fixing the machine in the top assembly. Normally there would be a fix or a fix and a bond constraint present.

Regards, **bleep**