Cancel
Showing results for 
Search instead for 
Did you mean: 

Condition Builder

Creator
Creator

Condition builder in NX9 is very good. We need one improvement to make it much better.

 

If we have an option to select the expression it would be great.

 

 

4 REPLIES 4

Re: Condition Builder

Valued Contributor
Valued Contributor

I never use the condition builder, but just type in the expression. That way you can double click the expression in the list and it is added to the expression your working on.

Using NX 8.0.3.4

Re: Condition Builder

Creator
Creator

But condition builder much better than typing in the expression editor. If I miss a bracket in expression editor I have to search and close.

In condtion builder I don't have to do those exercises.

Re: Condition Builder

Siemens Phenom Siemens Phenom
Siemens Phenom

Thadeus --

 

Good suggestion.  We'll look at implementing that.

 

In the meantime, I commonly use the Conditional Builder to build up the conditional LOGIC (including all of the necessary brackets), and then come back out into the main dialog to populate the actual references to other expressions. That way, I can take advantage of either typing completion, or the MB3-Insert, or the double-click operation to insert expression names as aluminum2 has described.

 

Thanks again for the ER!

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Condition Builder

Creator
Creator

Thnaks Andrew.

 

I do something different. Copy the expressions in notepad and paste wherever necessary in condition builder