Cancel
Showing results for 
Search instead for 
Did you mean: 

Constraint icon

Phenom
Phenom

Hello,

 

Does anyone know what the yellow box behind the check box means on the constraints in assemblies? I do not recall seeing it before. 

 

Thanks,

 

 

constraints.PNG

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM
4 REPLIES 4

Re: Constraint icon

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @TechniCsNC,

It means that constraint is arrangement spcific. Right click on constraint and you will see it.

Re: Constraint icon

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

if i'm correct it means that this constrains is also controled in an assembly arrangement.

 

With Assembly arrangement you are able the set an assembly in different possition or suppres some constrains.

 

arrangements

 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Constraint icon

Phenom
Phenom

Thanks guys. I have not used arrangements much, but I did use them on on this part. I do see the info when I right click. 

 

 constraints_specific.PNG

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Re: Constraint icon

Honored Contributor
Honored Contributor

We've had that icon show up, when arrangements weren't being used, at least intentionally.  My assumption has been that an arrangement was created at somepoint, maybe during a users experimentation/exploration of NX, but never utiliized, and the tag to trigger that icon is lingering.  It was never a big enough concern to submit an IR to GTAC.

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10