Cancel
Showing results for 
Search instead for 
Did you mean: 

Consultation regarding NX30120 NX Viewer license

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello,

 

I wonder if this license allows me to open igs, stp and dxf/dwg files.
I wonder if I can also calculate the weight of solid bodies.

If this license does not have these capabilities, what minimum license needed for this?

 

Thanks

Mikel

3 REPLIES 3

Re: Consultation regarding NX30120 NX Viewer license

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

No STEP, IGES or DXF/DWG. Yes to measure bodies for mass calculation. One of the Mach 1 bundles will have the translators in it.

Anthony Galante
Senior Support Engineer
PhoenxPLM

Re: Consultation regarding NX30120 NX Viewer license

Valued Contributor
Valued Contributor

Can I use the NX viewer without a license? (like Solid Edge, Catia, Solid Works......)

 

 

 

Re: Consultation regarding NX30120 NX Viewer license

Legend
Legend
No, The Viewer for NX requires a License.


I cannot remember the exact product, but there used to be a license that you could import step/iges/DXF as well as view NX files and it was less expensive than the NX viewer license.

Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro