Cancel
Showing results for 
Search instead for 
Did you mean: 

Continuous weld on gap

Phenom
Phenom

Hi,

it's possible (automatic method) without select all edges from set face 1 and set face 2 have a continuous weld on gap ?

Attached files.

weld.png

Thank you...

Using NX1876
RuleDesigner PDM

2 REPLIES 2

Re: Continuous weld on gap

Phenom
Phenom

Hi @SamadhanGaikwad ,

attached the image.

Thank you...

Using NX1876
RuleDesigner PDM

Highlighted

Re: Continuous weld on gap

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @cubalibre00 ,

 

As far as I know, you'll have to select all face/s in Set 1 and Set 2 in turn all edges to create a Weld.

It seems that there is no provision in dialog to create a continuous weld when there is a gap.

You can think of openeing an IR to neglect a gap on the faces with some provision, if you encounter with this situation often.

Otherwise your current workaround of using a Move Face is good one.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!