Cancel
Showing results for 
Search instead for 
Did you mean: 

Contour Flange does not work ?

Genius
Genius

Hello

How to create double flanges to a corner with Contour Flange ?

  • I get an error. Tried Single curve and Tangent curve in advanced selection.
  • I'm new to these contour flanges. It does not like the corner somehow.

"Chain section must consist of one or more connected edges with line or arc geometry. Edge with arc geometry must be tangentially connected with adjacent edge."

fsfsfs.jpg

ererrte.jpg

6 REPLIES

Re: Contour Flange does not work ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

To me it looks like the bend is too small to accomodate the flange and i am even more dubious if the flange can really be created on a bend like you mentioned. We have sheet metal utilities for treating corners like this but getting a combined flange (including the bend ) looks like more of forming operation to me...

Sheet metal experts can throw some light on it.

Regards

Kapil

Re: Contour Flange does not work ?

Genius
Genius

I can do it by creating 2pcs seperate flanges.

  •  and modifying the 45*degree in flanges.

jkkjkjkj.jpg

sdsfgg.jpg

dddfd.jpg

Re: Contour Flange does not work ?

Phenom
Phenom

The highlighted edge in the image would not be there. This means that the part is not well modeled.

Re: Contour Flange does not work ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Your methodology is fine...i think i got it wrong the first time ....You meant you wish to create the flanges (with the proper corner treatment ) in one single shot... I will not use a contour flange for this (until and unless the edge is curved one or the flange is not a straight one)...flanges are good to tackle it.

Best Regards

Kapil

Re: Contour Flange does not work ?

Gears Legend Gears Legend
Gears Legend

Hi 12131444,

 

I see a split face that might be the cause for the failing contour flange. (edit: I think Cesare is meaning the same thing)

 

2017-05-13_03.gif

I suggest to try to delete that small face. If deleting does not work, you might also want to try "replace face".

That's a very powerful synchronous tool.

After that you should get something looking like this:

2017-05-13_04.gif

 

Then try again. I'm pretty confident that it will work now.

In NX11 the result could look like this: (preview is not that OK)

2017-05-13_05.gif

and the flat pattern view then looks like:

2017-05-13_06.gif

 

I hope this could do the trick for you.

 

 

Huysmans Metalen n.v.
2x NX 12.0.2.9 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend

Re: Contour Flange does not work ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @12131444

Frank is correct, the input geometry looks like an extra face exists.  If this part was imported, try cleanup or re-create, contour flange should work OK there...

2017-05-15 11_34_26-NX 12 - Sheet Metal.jpg