Cancel
Showing results for 
Search instead for 
Did you mean: 

Control of "site" NX defaults

Gears Phenom Gears Phenom
Gears Phenom

We are using the NXcustom setup that Rob Cohon originated.  As things are, any user could change defaults at the "site" level, and I would like to lock this down.  Is this simply a windows permissions issue, regarding the folder containing the "nx90_site.dpv"?  or is there a better way?

 

Thanks,

 Dave

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
1 REPLY

Re: Control of "site" NX defaults

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes, it is a permissions issue. The users need to have "read" but not "write" permission to the file and/or the folder that contains it.