Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Convert interpart expressing to a constant

Experimenter
Experimenter

Hi,

How do I convert an existing interpart expressing to a constant?

 

 

I'm using  NX 12.02.2.9 MP1

 

tag: inter part expressing

7 REPLIES 7

Re: Convert interpart expressing to a constant

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

You need to create another Number expression with unit set as constant, and in it's formula put the interpart linked expression name.
I can give more detailed information if you send a screenshot of your expressions.  

Re: Convert interpart expressing to a constant

Experimenter
Experimenter

Hi

Here is a screenshot.  I'm new to NX12.  We just upgraded from NX 8.5.  Before I would just type over the text "<part name>::<expression>" with the number 2.   Now I can not figure out how to type in that field.

 

Note the part is PB_123_32_PN.prt is not loaded.  The part is "lost".  "Or very hard to find".   

 

5-14-2019 5-30-09 PM.jpg

 

 

Re: Convert interpart expressing to a constant

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Annotation 2019-05-14 145407.jpgConverting removing units from a interpart expression

Re: Convert interpart expressing to a constant

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Not sure if you would be able to link by using "<part name>::<expression>"  if the other part is saved in a different folder.

Are you in managed mode or unmanaged mode ?

Re: Convert interpart expressing to a constant

Experimenter
Experimenter

Hi 

We are using SAP ECTR. 

Maybe there is some confusion.  

I want the expression   DG1_0 = 2

 

Right now DG1_0 = "PB_123_32_PN":Smiley Very HappyG1

and I want it to be 

DG1_0 = 2

 

Re: Convert interpart expressing to a constant

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Oh, that should be simple. 
Select the expression that you want to change value and Click on Edit interpart expression under Actions(left tab). 
it will give you options to select the Part, select the part and click on delete reference , and do OK , now you should be able to change value of your expression.

Re: Convert interpart expressing to a constant

Experimenter
Experimenter

Hi m1-G

That worked.   I pick the one under Actions with the text says:

"Edit Multiple Interpart Expressions"   

Then I could pick the part

"Delete Reference"

 

That turned the value into a constant. 

It is now DG1_0 = 2

DG2_0 = 2

 

Thanks !!