Cancel
Showing results for 
Search instead for 
Did you mean: 

Converting Units on export

PLM World Member Creator PLM World Member Creator
PLM World Member Creator

Hello All,

 

I have a part designed in Inches.  I'd like to export it out as a step file in mm.  Is this possible?  If so, how?

 

Thanks

 

Jerry

 

NX9.0.3.4 MP13

4 REPLIES 4

Re: Converting Units on export

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Hi Jerry,

There does not appear to be an option on the UI or in the settings file.

You could use the following workaround:
Create a new millimeter part file and use "File > Import > Part" to import your inch part. You will get a "Metric-English units conflict, automatically scaling part" message. Choose OK and then export the geometry using the STEP translator. Perhaps someone has a better solution?

Regards, Ben

Re: Converting Units on export

Legend
Legend

Hi Jerry,

 

You can use the ug_convert_part.exe.

This file is found in UGII folder and must be executed with Command Prompt.

This executable file can convert your part from inch to mm or vice-versa.

 

Below the link with more information.

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:xid280845

 

After you convert your part, you can export to STEP.

 

I hope this help.

Jean Marcel
PLMPRO
www.plmpro.com.br

Re: Converting Units on export

Experimenter
Experimenter

Re: Converting Units on export

Experimenter
Experimenter

JUST CHECK WITH LINK YOU WILL GET THE SOLUTION