Cancel
Showing results for 
Search instead for 
Did you mean: 

Converting assembly to solid part body?

Experimenter
Experimenter

Hi,

 

Does anyone know how to create a single, airtight solid body from an assembly that preserves the exterior details while removing the interior details? This is what the old Simplify Assembly command did in NX8,5. unfortunately it is not longer available in my NX11.

 

Probably it is a whole job to do it manualy. So I already would be happy if I could just convert the assembly to one solid body file.

 

Thanks for the prompt reply.

Rollin.

4 REPLIES

Re: Converting assembly to solid part body?

Genius
Genius

I don't know if there is a specific command in Nx for that. If it doesnt exist I thinki it should. A workaround would be to disasociate wavelink all bodies in the assembly to the general assembly part and then use booleans to unite all the bodies.

Re: Converting assembly to solid part body?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

I guess you can still access "SIMPLIFY ASSEMBLY". Use command finder to search for the same (i have just checked it in NX11 ...but not 11.0.1 yet).

Best Regards

Kapil

Re: Converting assembly to solid part body?

Siemens Phenom Siemens Phenom
Siemens Phenom

I just checked and it is still in NX 11.0.1. 

 

Scott

Re: Converting assembly to solid part body?

Siemens Phenom Siemens Phenom
Siemens Phenom

Simplify Assembly is on the Assemblies ribbon-->More-->Advanced

2017-04-26 09_17_47-NX 11.0.1.11 - Modeling - [sheet_metal_bracket.prt (Modified) ].jpg

2017-04-26 09_16_26-NX 11.0.1.11 - Modeling - [sheet_metal_bracket.prt (Modified) ].jpg

Command Finder is your friend.