Cancel
Showing results for 
Search instead for 
Did you mean: 

Coordinate driven curve

Phenom
Phenom

If I get hundreds of XYZ coordinate points, how could I insert those points in a model to create a curve?

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

5 REPLIES 5

Re: Coordinate driven curve

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you have a text file that lists point coordinates, you can use "import points from file" to create points in your NX file. Now that you have point objects to work with, you can use "fit curve" to create a curve from the points.

Re: Coordinate driven curve

Phenom
Phenom

Is it possible to import the coordinate table directly to generate the curve?

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Coordinate driven curve

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Unfortunately, no.

Re: Coordinate driven curve

Siemens Phenom Siemens Phenom
Siemens Phenom

It is possible.

There is still an old spline functionality, which is about to be retired... But still available in NX10.

Use the command finder and look for "spline retire" and you'll find it.

The usage is very very old fashioned, but it should work.

 

Regards,

Johannes

Re: Coordinate driven curve

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Mike,

You can use Knowledge fusion also besides the method elaborated by Johannes. I had an old code that might work in latest versions also but will have to look for it.

Best Regards

Kapil