Cancel
Showing results for 
Search instead for 
Did you mean: 

Copying holes

Valued Contributor
Valued Contributor

I do this with syncronous by copying face and then cutting the body or with geometry pattern and then cutting the body. Is there a direct way of copying directly the hole? 

I want to do that because after that I want to apply a threaded hole but doing that in drafting I see the threaded hole geometry and the copied surface geometry, so I have to manually delete surfaces after applying threaded hole, but I sometimes forgot. I cant use feature pattern because I dont want to copy all holes in the feature.

1 REPLY

Re: Copying holes

Siemens Phenom Siemens Phenom
Siemens Phenom

Can you post an image of the staring point and ending point? I would like to see what are trying to accomplish. There maybe a better way to get the results you need. As for the drafting part you should look at reference sets to control what shows up on the drawing sheet.

 

Scott