Cancel
Showing results for 
Search instead for 
Did you mean: 

Counterbore holes

Creator
Creator

Dear All,

 

Is it possible to make a table with standard couterbore holes in order to simply place these as feature in a model?

 

I find it strange and a pity that this is not standard integrated in the hole comment. Now I every time have to look up and change these values manually.

 

Regards, Michel

4 REPLIES

Re: Counterbore holes

Genius
Genius

Standard size Counter bores are listed in the hole command.

Kurt Neubaecker
CAD/CAM Designer
Proficient Industries
Cleveland, Ohio

Re: Counterbore holes

Phenom
Phenom

With the Hole command, make sure you select a Type = Screw Clearance Hole. Then select a hole Form = Counterbored.

 

With those set, choose a Screw Size and Screw Type. The Counterbord parameters are automatically filled in.

 

There was a thread earlier about how to change the table values.

 

 

 

Re: Counterbore holes

Phenom
Phenom

If you want to customize your C/B hole sizes, edit the following (Make sure to save a copy for recovery)

…\NX xx.x\UGII\modeling_standards\nx502_Screw_Clearance_Hole_Standard.xml

 

When you restart NX, it will use new values.

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Counterbore holes

Creator
Creator

Thanks a lot all. I should have looked betterSmiley Embarassed.

 

Also nice to know how to change the table values.

 

Michel