Cancel
Showing results for 
Search instead for 
Did you mean: 

Create additional leaders for an existing drawing note in NX 8.5

Experimenter
Experimenter

Hi.  Can't seem to create additional leaders for an existing drawing note in NX 8.5.  Is it so simple that I'm overlooking it?  Possibly can't be done?  Thanks.

4 REPLIES 4

Re: Create additional leaders for an existing drawing note in NX 8.5

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Edit the note; in the note dialog, expand the Leader -> List section. Choose "new" from the list and select a leader location on the drawing; a new leader will be added to the note. I think there is (or was) a limitation of 9 leaders on one note object.

Re: Create additional leaders for an existing drawing note in NX 8.5

Experimenter
Experimenter

That did it.  Thanks very much cowski1!

Re: Create additional leaders for an existing drawing note in NX 8.5

Siemens Phenom Siemens Phenom
Siemens Phenom

A quicker way to add leaders to an existing note is to first double-click the note to place it in Edit mode, and then right-click in the background of the graphics window and choose Add New Leader from the shortcut menu.

Re: Create additional leaders for an existing drawing note in NX 8.5

Experimenter
Experimenter

Thanks DEckhoff.

Just gave your method a try.  Works great, thanks.