Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating 3D PDF file using NX 10

Experimenter
Experimenter

Dear All,

 

As iam fresher to UG NX, i want know how to create 3D PDF file in NX 10 version. I tried with FILE-export-PDF. but it works only for 2D drawings. please let me know the solution.

 

Thank You.

2 REPLIES 2

Re: Creating 3D PDF file using NX 10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NX10 does not directly support creation of 3D PDFs - you have to use some external software (If you search this, or the "NX Customization & Programming" forums, you should see some discussion on this)

 

Starting in ?NX1847? or later, 3D PDF creation is directly supported in NX (but it needs a license)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Creating 3D PDF file using NX 10

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Harish_Dhavali 

It was introduced in NX 1847 so there is no option in any previous release/version.

Publish Technical Data Package