Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating PDF - sorting sheets

Genius
Genius

Hello, I have a multi-page drawing that I'm trying to create a PDF of.  When I go to export the PDF, it orders the sheets 1,10,11,12, etc. and then does 2, 21,22...   Is there a way to set up the export PDF creation process so that I don't have to reorder them myself?  Thanks

7 REPLIES

Re: Creating PDF - sorting sheets

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @s_hightower,

 

Which version of NX are you using and what do you have the Sort Order set to in the Customer Defaults?  In NX11 it is set to Alphabetical by default.

From the Customer Defaults, select "Gateway > PDF Export" and see if changing the 'Sorting Order' to 'Numerical' makes a difference for you.

 

Regards, Ben

Re: Creating PDF - sorting sheets

Genius
Genius

Hi @BenBroad, We're using NX 10.0.3.5.  

 

I selected Gateway and noticed that "Gateway" is now part of the Title/Header at the top of the screen.  I can't find the "Gateway > PDF Export".  All I can find is "File > Export > PDF".   It's possible that I'm just overlooking the command.  Any recommendations?

 

 Gateway.JPGGateway at top of screen

Thanks for your help.

 

Re: Creating PDF - sorting sheets

Siemens Phenom Siemens Phenom
Siemens Phenom

File > Utilities > Customer Defaults.

 

cd.PNG

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Creating PDF - sorting sheets

Genius
Genius

That worked!  Thanks, everyone, for your help!

Re: Creating PDF - sorting sheets

Experimenter
Experimenter
I've changed default to numerical. When exporting I still get the 1,10,11...2,20,21..... Smiley Sad

Re: Creating PDF - sorting sheets

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@erickel wrote:
I've changed default to numerical. When exporting I still get the 1,10,11...2,20,21..... Smiley Sad

Did you restart NX after making the change in the customer defaults?

Re: Creating PDF - sorting sheets

Experimenter
Experimenter

I just did. Perfect!

Thanks!