Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating a Symbols Library in Teamcenter

Experimenter
Experimenter

Hello,

 

We are running a managed environment in Teamcenter and NX 8.5. I would like to create a global custom symbols library which can be accessed by any employee using NX through Teamcenter. Any employee should be able to create custom symbols and populate the library and it should be available to everyone else. How would I go about creating something like this?

 

Thanks in advance.

1 REPLY 1

Re: Creating a Symbols Library in Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Well, if any employee can create symbols, after a while you'll have chaos ;-)

 

This can be done in folders in TC (set in site or group customer defaults), but the problem is if a user wants a "user level" folder for their re-use library, it over-rides the site one.

 

I believe you need to (or at least want to) look at using classification (in TC) for your re-use library. 

Unfortunately we haven't gotten to that point yet, so I can't offer any help.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled