Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating a helical-style groove on a non-circular face - NX12

Experimenter
Experimenter

Hi Everyone,

 

I am trying to create a groove that has a helical profile along a surface that has a non-circular face, almost elliptical.

 

The closest I have got is shown in the attached file

 

If anyone has a solution then please let me know!

 

Any questions, please ask.

8 REPLIES 8
Highlighted

Re: Creating a helical-style groove on a non-circular face - NX12

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @JL95 

Project helix curves, then create sweep feature using projected curve and subtract it from target solid body.

 

(view in My Videos)

Re: Creating a helical-style groove on a non-circular face - NX12

Siemens Phenom Siemens Phenom
Siemens Phenom
What is wrong with the example you attached ?
- Knowing that might help us provide ideas... :-)
also, if you can upload actual geometry or descriptive illustration , it would help.

Regards,
Tomas

Re: Creating a helical-style groove on a non-circular face - NX12

Experimenter
Experimenter

Thanks for the quick reply Ganesh!

 

Your model is good thank you!

 

Is there a way to keep the grooves parallel like on the model I have attached, as in, to avoid the 'wavy' bits on the top and bottom?

 

Many thanks,

Re: Creating a helical-style groove on a non-circular face - NX12

Experimenter
Experimenter

Hi Tomas,

 

The example I attached was quite complicated to model and I was hoping for a better solution :-)

 

Thanks, I will keep that in mind for the future!

 

 

Re: Creating a helical-style groove on a non-circular face - NX12

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @JL95 ,

Try changing Projection direction from 'Toward line' to 'Along vector' and select 'YC'. It might help.

HelixProjection.PNG

Thanks,

Amol

 

Re: Creating a helical-style groove on a non-circular face - NX12

Experimenter
Experimenter

Hi Amol,

 

Unfortunately this doesn't work as intended, the curves 'break' with these settings applied.

 

Thanks,

Re: Creating a helical-style groove on a non-circular face - NX12

Siemens Phenom Siemens Phenom
Siemens Phenom
jl95 : you did not tell how you modeled your version. we do not know that. :-)

The wavy shape is resulting from the fact he projects a helix onto a flat face, it's the natural resulting shape.
If you want straighter lines, either you find a method of creating a non-cylindrical helix , or model the zig-zag shape differently.

Amolkadam, i think you are confusing the methods used when creating a swept surface with this projected curve, Vector in this case will simply project the curves in a given direction and not concentric towards a center placed line.

Regards,
Tomas

Re: Creating a helical-style groove on a non-circular face - NX12

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If the projection vector doesn't work, then try creating 2 guide curves (top & bottom of the groove at the outer surface) & see if they work better

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled