Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Cura interface to NX

Legend
Legend

Cura 3.0.4 provides a pluggin for NX to provide a direct interface in the NX ribbon.

The problem I have is that when I click the button, I get

 

License Error, License Module Not Found [-10005]

 

Does anyone know if there is a special license for this?

Or is my problem due to using the Learning Edition?

 

Export STL works ok. But it would be nice to get this new interface to work.

 

cura_interface.jpgCura interface

3 REPLIES

Re: Cura interface to NX

Phenom
Phenom

Hi @MarkLawry,

I'm the Cura interface also and the tool to export to Cura works fine. The Cura button use a journal to interface to the Cura software. Learning License doesn't have the journal run module maybe.

Thank you...

Using NX 11 / RuleDesigner PDM

Re: Cura interface to NX

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

i have created with a colleague the NX interface for ultimaker.

 

There is no check for license in the tool. 

It only can be that you don't have a runtime license voor journals


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Cura interface to NX

Legend
Legend

That has to be the problem. Correct, I believe the Learning Edition does not include Journaling.

 

Anyway, it is nice to see the Cura interface in NX. There have been other questions on in the past on this forum where that should have been the answer. 

 

Thanks for the response.