Cancel
Showing results for 
Search instead for 
Did you mean: 

Customize B.O.M

Creator
Creator

I was wondering if anyone had information on how to Customize the Standard B.O.M (Parts List) when creating drawings. I would like to have more columns in the table, right now I have to do it each time I create the "Parts List". I would like to have a standard file that everytime I click the "Parts List" it will automatically bring in mine and fill all the columns with the attributes.

 

I would like to add in:

-Material

-Overall Size (if there is an attribute that can calculate that for me and put it in so i dont have to fill it out manually)

-Weight

 

Any information would be greatly appreciated

 

Thank You

16 REPLIES 16

Re: Customize B.O.M

Creator
Creator

Also Does anyone know when Importing a view if it can automatically put whether its the "Top View", "Bottom View", etc. Just like when you create a section view it automatically names its.

 

Thanks

Re: Customize B.O.M

Phenom
Phenom

I've customised the BOM (=Parts List) and it's working quite well.

 

Follow instructions: https://docs.plm.automation.siemens.com/tdoc/nx/10.0.3/nx_help/#uid:index_tcint:id1299826:xid454367Smiley Tonguea...

 

  • Re structure the NX default Part List
  • RMB the new list and "Save it as a Template" under.../GUII/table_files (_metric or _english postfix will be automatically added by the system)
  • Define Parts List location under Customise Darafting Standards >Table>Patrlists>Format. 
  • chanage environment variable: UGII_IGNORE_INTERNAL_PLIST=1
  • restart NX

 

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Customize B.O.M

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Have a look at the video I created a while back on parts lists: https://vimeo.com/album/3065578 It covers how to create & modify parts lists. There should also be a video among them on putting weigh in the BOM.
Anthony Galante
Senior Support Engineer
PhoenxPLM

Re: Customize B.O.M

Creator
Creator

I followed the video to put in the weight but its not showing anything. Do you have to have the right license to be able to do it?

Re: Customize B.O.M

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You shouldn't need a special license. As long as the parts have a mass, it will work. Have a look at which explains how mass data can be generated for a part: https://vimeo.com/106898990
Anthony Galante
Senior Support Engineer
PhoenxPLM

Re: Customize B.O.M

Creator
Creator

Okay I got the weight figured out (Thank You)

I got the NX Material put in as well. My only issue now is overall size of the item.

When I go to "Check Regions" -> Select the "Calculate" icon -> Then "Information" Tab -> Select "Model Properties" it gives me the Diemnsions of the Model (X, Y, Z). How do I make that show in my "Parts List" or is it not possible? If it can generate the overall size then it should be able to import that into the "Parts List". I cant find anything showing how to do that.

 

I know the Check Regions is a Mould Wizard thing but I use that to show faces that arent drafted, crossover faces and things like that. 

 

 

Re: Customize B.O.M

Creator
Creator

Thank You

Once I get everything I want in my Parts List I will follow this step

Re: Customize B.O.M

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi, I am JoDi, Indonesian Siemens Partner.

Do you have any idea how to Customize the spreadsheat in Bill of Materials?
My customer wants to customize spreadsheet template in BOM.

Highlighted

Re: Customize B.O.M

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

@JoDi wrote:

Hi, I am JoDi, Indonesian Siemens Partner.

Do you have any idea how to Customize the spreadsheat in Bill of Materials?
My customer wants to customize spreadsheet template in BOM.


 

Hi JoDi,

 

By "Bill of Materials", are you referring to the Drafting Parts List?  The reason I ask is that you cannot use the Spreadsheet functionality to edit Parts Lists, similar to how you can with Tabular Notes.  Are you able to give us any more information so that we may try to help you?

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration