Cancel
Showing results for 
Search instead for 
Did you mean: 

Cut/Trim pattern elements of workpiece CAD

Creator
Creator

Hello,

 

I wanted to cut/trim/subtract two pattern elements from my workpiece, but get an error report (See Image and prt-File).
In the discussion forum i couldn't find any help.
Is there maybe an alternative way to do this kind of operation?
Can i get the finished workpiece in .prt or .slt format?

 

 

 

Sincerly Rick

11 REPLIES

Re: Cut/Trim pattern elements of workpiece CAD

Legend
Legend

Why is it a Pattern Feature and not a Swept Feature?

Re: Cut/Trim pattern elements of workpiece CAD

Legend
Legend

swept.jpg

Re: Cut/Trim pattern elements of workpiece CAD

Siemens Phenom Siemens Phenom
Siemens Phenom

@RickTick: Use 'Sweep Along Guide' command to create the feature and within command there is a boolean option to subtract the same feature from the cylinder. Now in your part, Pattern Feature(13) has 412 instances, Pattern Feature (14) has 378 instances. This has increased the file size and it is not easy to deal with it. Updating features take considerable time.

 

Now the error you are facing while doing a subtract operation is because, instances of pattern features are independent, not united together. Use Sweep Along Guide command and check the result.

 

pt.PNG

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Cut/Trim pattern elements of workpiece CAD

Phenom
Phenom

If you've tried to simulate a milling operation, considering that you just make a revolve using the sketch curve and the normal vector of the arc.

 

Re: Cut/Trim pattern elements of workpiece CAD

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Did you also try sweeping a tool solid along the path. There is a special operation for that: swept volume.

 

Regards, **bleep**

(view in My Videos)

 

 

Re: Cut/Trim pattern elements of workpiece CAD

Creator
Creator

@Cesare

Yes i want to simulate a milling operation. If i revolve my sketch i dont get the surface roughness of my workpiece and i cant determine my discretization, because of that i used pattern elements.

 

 

Re: Cut/Trim pattern elements of workpiece CAD

Creator
Creator

@DickBaardse i cant find this command in NX9.

Re: Cut/Trim pattern elements of workpiece CAD

Creator
Creator

@joewhite i want to simulate the surface roughness of my workpiece

Re: Cut/Trim pattern elements of workpiece CAD

Genius
Genius

I think sweep body is a NX11 feature