Cancel
Showing results for 
Search instead for 
Did you mean: 

DEFORMABLE COMPONENTS LICENSE

Valued Contributor
Valued Contributor

Hi,

 

Does anyone knows if Deformable components are available in Mach Advantage License?

 

I mean, can I create and use deformable components with a Mach Advantage?

 

Thanks in advance!

 

 

2 REPLIES

Re: DEFORMABLE COMPONENTS LICENSE

Siemens Phenom Siemens Phenom
Siemens Phenom

Other then being able to create an Assembly and Feature models, I don't think there's any other requirement.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: DEFORMABLE COMPONENTS LICENSE

Siemens Legend Siemens Legend
Siemens Legend

Hi,

 

Deformable Component Definition comes with the User Defined Feature License, and this one is not included in Mach Advantage.

To verify, please look into the license log of the license server. If it does not include a DENIED entry, set the variable FLEXLM_DIAGNOSTICS=3 on the NX client machine. This will report any request from NX to the license server that is not available (not all of them are errors).

 

Johannes