Cancel
Showing results for 
Search instead for 
Did you mean: 

Deactivation of thread cut lines possible?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi all,

Does anyone know if there is a setting to deactivate the auto creation of thread cut lines (Geman: Gewindeanschnitt) in NX?

When creating a thread hole, these lines will automatically be displayed in a section view. We want to deactivate these lines by default for specific drawings.

Default representation in NX:

NX.png

 

 

 

Comparison: Solid Edge will not display these lines by default:Solid Edge.png

 

Regards,

Nico

9 REPLIES 9

Re: Deactivation of thread cut lines possible?

Siemens Phenom Siemens Phenom
Siemens Phenom

Why?

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Deactivation of thread cut lines possible?

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @bct_nschmid,

 

I couldn't find an option to show/hide the thread runout in NX, but after much searching I did find the following regarding the representation - Drafting conventions associated with threads:

 

Screenshot - 6_28_2018 , 9_53_59 AM.png

 

"Note. the line at 30° indicating the runout was the practice in BS 308:1972. However, in 1984 the revised standard permitted the line to be omitted if there was no functional need."

 

If it's important for you to remove them, you can view dependently erase them.

 

Regards, Ben

Re: Deactivation of thread cut lines possible?

Siemens Phenom Siemens Phenom
Siemens Phenom

More importantly, if you can site a standard, then that would be a legitimate basis for an ER.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Deactivation of thread cut lines possible?

Phenom
Phenom

image.png

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Deactivation of thread cut lines possible?

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Thanks @mike_fdo.  I spend considerable time scouring the internet for something concrete - the closest thing I found was the information I provided above, and the following:

 

Screenshot - 6_28_2018 , 9_07_06 AM.png

 

 

It could have be coincidental, but whenever I my search string included "ANSI", the thread runout was not shown and when searching ISO it was.

 

Regards, Ben

 

Re: Deactivation of thread cut lines possible?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@mike_fdo, what standard or publication did the scan come from? The "cf." in the note at the top of the page is directing the reader to compare what is shown to DIN 406-11 and DIN ISO 6410-1, which implies that the scan is from neither of those standards.

Re: Deactivation of thread cut lines possible?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi all,

at first, let me thank you for all the information.
We also got the information from one of our customers, that the thread cut lines may be omitted. They need this in order to get a clearer representation of some of their drawings.

 

Looks like there really is no setting yet, so I think we will raise an ER for this.

 

Regards
Nico

Re: Deactivation of thread cut lines possible?

Phenom
Phenom

@cowski1; It's from Mechanical and Metal Trades Handbook 45th Edition, 2011; ISBN 13 978-3-8085-1914-1

 

When googled;

image.png

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: Deactivation of thread cut lines possible?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Good info, thanks @mike_fdo.