Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Decimal places of Attributes

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi there,

 

Is there a way to change the number of decimal places of the attributes?

 

For instance, I'm using MY_MASS linked to NX_MASS, so when I import it to the drafting the NX show every decimal places possible.

1 REPLY 1

Re: Decimal places of Attributes

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @bauler,

 

Please refer to page 4 of this thread.

 

Currently the only way to control the decimal places is to use a tabular note to display the values.  Use "Edit Text" and then the Relationships option to point to the Part Attribute and then use "Settings" to change the Cell Category to Number and then you can edit the Decimal Places.

 

ER 7607101: "Unable to control the precision of Attribute Template values"

You could also create an expressions to read the attribute value and truncate it, but I suspect that you might have to force any updates using that method.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration