Cancel
Showing results for 
Search instead for 
Did you mean: 

Delete project curve

Phenom
Phenom

Hi,

on NX8 the delete button on project curveS, it permit to delete the entire curveS. Now in NX10 I'm not able.

Idea / solutions ?

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

1 REPLY

Re: Delete project curve

Siemens Phenom Siemens Phenom
Siemens Phenom

I see NO difference in behavior between NX 8.0 and NX 10,0 when it comes to deleting the curves of a Project Curve feature.  Note that the only way that you can delete less than ALL the curves of a Project Feature is IF the Project Feature was NOT created with the 'Associate' option toggled ON.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA