Cancel
Showing results for 
Search instead for 
Did you mean: 

Design Validation for Additive Manufacturing

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

I saw a video where the analysis tools Design Validation for Additive Manufacturing have been shown.

How can I activate this group of commands in NX12?

 

2019-01-15 12_26_37-Design validation.png

7 REPLIES 7

Re: Design Validation for Additive Manufacturing

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @juraj_zahradnik,

If you open existing AM part or create new one from File > New > Additive Manufacturing tab, then you will be able to see that group under analysis tab.

Re: Design Validation for Additive Manufacturing

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

other wise these checks are located in a new tab in NX 12 the Design for AM tab.

so they are moved from the analysis tab to this new one. 

The new one also contains lattice and Print CSYS.design_4_AM_Tab.JPG


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Design Validation for Additive Manufacturing

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

I seem to recall that you also need to install NX 12.0.1, at the minimum.  Currently NX 12.0.2 is available, so I'd probably go with that MR.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: Design Validation for Additive Manufacturing

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi all,

thak You for hints.

I have installed the NX customized, not all features have been installed (NX becomes larger and larger).

I have installed only these features:

2019-01-17 06_12 Features.png

And I guess that the Design Validation can be part of Validation or Manufacturing Planning.

Re: Design Validation for Additive Manufacturing

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
I have NX 12.0.2.9.

Re: Design Validation for Additive Manufacturing

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
I can not even find any command of this command group in NX.

Re: Design Validation for Additive Manufacturing

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Yes - I have it, these functionalities are part of Validation instalation feature of NX12.