Cancel
Showing results for 
Search instead for 
Did you mean: 

Designing a warning sign 3D-model ?

Genius
Genius

Hello

What license if any do I need to place a photo of a warning sign inside NX11 ?

  • Now I'm drawing it by myself from scratch...Hard times because edges have 4pcs of Jogs.
  • How to create texts and borders that follow the jogs without using any Extruding ?
  • I also need to color those areas afterwards.

lines424.jpg

5 REPLIES 5

Re: Designing a warning sign 3D-model ?

Genius
Genius
Someone told me to create the sign as a "solid model" from the start and Cut\Extrude the corners instead of Jogs ?

Re: Designing a warning sign 3D-model ?

Phenom
Phenom
have you looked into using project curve onto your surface, then use divide face, then select these faces, and color them. When you project curve you have options, along vector, normal to surface. I would try along vector first.

Re: Designing a warning sign 3D-model ?

Siemens Legend Siemens Legend
Siemens Legend
What is the overall purpose of this ?
A 3D warning sign, where different colors appear depending on the "thickness" ???
another trick could be placing the text , say 0.1 mm above the plate, then extrude the text, distance = 0
- will create Sheet bodies.
Regards,
Tomas

Re: Designing a warning sign 3D-model ?

Genius
Genius

Project curve did it !

I made a sketch then I made a 2nd sketch and there I used Project curve to project the 1st sketch.

Working.

project curve.jpg

Re: Designing a warning sign 3D-model ?

Phenom
Phenom

Is this what you are looking for?

image.png

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW