Cancel
Showing results for 
Search instead for 
Did you mean: 

Detailed threads

Phenom
Phenom

Is there anyway to disable them?  Experience has shown no added benefit other than they look cool.  On the other hand the machine shop hates them when programming, drawings look cluttered, etc.

 

 

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
1 REPLY

Re: Detailed threads

Siemens Legend Siemens Legend
Siemens Legend

If you are using the Thread command then simply select 'Symbolic' as the Thread Type. You must do this for every hole. If the detailed threads already exist, then you need to delete each thread feature and create a new Symbolic thread. Because this is a very old command which does not use a block based UI, the edit dialog is not the same as the create dialog.

 

Better yet, you should always use the hole command to create threaded holes.

 

There is no global setting to show detailed vs. symbolic.

 

Abe

Regards,
Abe