Cancel
Showing results for 
Search instead for 
Did you mean: 

Dia symbol size

Gears Phenom Gears Phenom
Gears Phenom

OK, I have one drawing with tiny little dia symbols, and I can't find the setting to adjust the size.  I'm guessing it's a ratio of some sort, but where?

 

Thanks,

 Dave

-Dave
NX 11 | Teamcenter 11 | Windows 10
8 REPLIES

Re: Dia symbol size

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you saying that this 'Ø' symbol is part of a Diameter dimension or just when a symbol inserted in a note?  Could you provide a picture of the results that you're getting?  What font are you using?

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Dia symbol size

Gears Phenom Gears Phenom
Gears Phenom

Font is Arial Unicode MS

 

These just look really tiny, especially in the threaded hole callout.

 

TooSmall.jpg

 

This is from another drawing:

SeemsBetter.jpg

 

Seems like they used to be closer in size to the test.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Dia symbol size

Siemens Phenom Siemens Phenom
Siemens Phenom

You indicate that you're running on Windows 8.1.  Did you recently upgrade to Windows 8.1 or did you start with new system and install NX on it?  I ask because it's possible that you may not have the additional NX TrueType font libraries installed.  Go to the Windows 'font' folder and see if the following font files are found:

 

NX ANSI Symbols Italic

NX Constraints Regular

NX ISO Symbols Italic

 

If not, you may need to run repair on your NX 9.0 installation.

 

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Dia symbol size

Gears Phenom Gears Phenom
Gears Phenom

I have all 3 of those fonts, and this was a clean window 8.1 install.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Dia symbol size

Siemens Phenom Siemens Phenom
Siemens Phenom

Sorry, I wasn't able to reproduce the problem with NX 9.0 on Windows 7.  Note that this and many other symbols are not dependent on the font being used as long as it's one of the system installed TrueType or OpenType fonts.  You might want to give GTAC a call as it's possible others have reported this problem and know how to address it.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Dia symbol size

Gears Phenom Gears Phenom
Gears Phenom

Thanks John.

 

-Dave

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: Dia symbol size

Genius
Genius

We had the same problem on a few of our drawings when we changed over to ISO standards from ASME. Our new font is also Arial Unicode MS. We have a program to change all the annotation settings and rerunning this program cleared the problem. You may be able to update the drawing annotation settings manually to do the same.

Mike

NX 12.0.0 TC11.3 VMU 11.3

Re: Dia symbol size

Gears Phenom Gears Phenom
Gears Phenom

IR submitted, and it appears to be an issue with truetype font's.  It's going to development now...then maybe a PR.

-Dave
NX 11 | Teamcenter 11 | Windows 10