Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimension arrows inside IN ?

Genius
Genius

Hi

Dimension arrows won't go inside even when selected "IN" ?

 

Arrows inside.png

3 REPLIES 3

Re: Dimension arrows inside IN ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

The arrowhead size is too big to be accomodated inside the 10mm gap(even if it would have happened they would have overlapped).That is the reason why the "IN" does not work. Change the arrowhead size to a small size.

Best Regards

Kapil

Re: Dimension arrows inside IN ?

Siemens Legend Siemens Legend
Siemens Legend

 

I see you are on NX 9, Kapil's response is correct if you want the arrows to be inside in NX 9, however just for your information in NX 10 we added the jog option for narrow diemensions which if you upgrade you can take advantage of.

 

Regards

 

Paul

 

 

Jog Dimension.jpgNew Jog Option came in NX 10

Re: Dimension arrows inside IN ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Thanks Paul Smiley Happy  i did not know about it

Regards

Kapil