Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimension marking unit round issues

Pioneer
Pioneer

Moi,

 

We have a wired situation. In the drafting view, when we add the dimension into the drafting.

Some dimensions with ".5", (Exactly extra ".5")

When we used the setting => Text => Units => Decimal Places: 0

Some of the dimension is round up. For example: 143.5 => 144.

Some of the dimension is round down. For example: 1282.5 => 1282...

PS: In the same drafting. But when dimension 1282.6 => 1283...

 

Does someone else have the issues? It is quite wired...

 

Best wishes!

Edward

2 REPLIES 2

Re: Dimension marking unit round issues

Siemens Phenom Siemens Phenom
Siemens Phenom

@Edward1042 , Please add NX version as a tag in post. Is this issue with particular part or is a general issue?

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!
Highlighted

Re: Dimension marking unit round issues

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Edward1042 ,

Please go through below links. 

NX documentation:

Round-off rules for Drafting

Discussion thread regarding same topic.

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Rounding-in-drafting/td-p/301957

Regards,

Amol