Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimension style in NX 10 detailing

Experimenter
Experimenter

Please let me know how to achieve this dimension style in NX10.

 

1 REPLY

Re: Dimension style in NX 10 detailing

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @Mayureshpitre,

 

It looks like you're requirement is to create Angular Ordinate Dimensions (or Angular Running Dimensions), which is a current limitation of NX.  Existing Enhancement (ER) 7322951 asks for this functionality.  Similarly you can't create Chain or Baseline Angular dimensions (ER 2241378).

 

While Angular Ordinate/Running Dimensions can be mimicked it's probably not worth the time and effort to do so - it would be much quicker to create regular Angle dimensions.  Here's a mimicked example using manual dimensions and associating the appended text with sketch dimensions (amongst other things):

 

Screenshot - 4_18_2018 , 12_31_37 PM.png

 

Regards, Ben