Cancel
Showing results for 
Search instead for 
Did you mean: 

Dimension to the Control Point of Splines in Drafting

Pioneer
Pioneer

In NX 10 Drafting, the user was allowed to select an edge that was created by a Studio Spline Through Points and have the "Control Points" be selectable in Drafting Mode for dimension purposes. In fact, in NX 10, the "Knot Point" = "Control Point". 

In NX 11 Drafting, only "Knot Points" are viewable and they ARE NOT EQUAL to the control points, as I have shown in the attached picture. 

Has NX 11 lost the capability to dimension a spline's control points in the Drafting Application? 

 

Thank you,


Jeff Morris
RPI

4 REPLIES 4

Re: Dimension to the Control Point of Splines in Drafting

Pioneer
Pioneer

Further,

 

I have witnessed this same problem in NX 12.0.0.27 mp03

I've submitted an IR 8949704 and was told "there has not been a need for that functionality". 

I could not believe it. 

Re: Dimension to the Control Point of Splines in Drafting

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @rpipace,

 

Your IR was converted to a PR (Problem Report) back when you initially reported the issue.  It's currently under review by development.

 

Regards, Ben

Re: Dimension to the Control Point of Splines in Drafting

Pioneer
Pioneer

Thanks Ben. Just called GTAC an hour ago and they did confirm that exact detail. 

Re: Dimension to the Control Point of Splines in Drafting

Legend
Legend

Hi @rpipace

 

Just for workaround,

You can create  define point by point set command.

And use the (existing) define point to make drafting domension.

 

 

 Sunkap Ahn, Senior Support Engineer


logo