Cancel
Showing results for 
Search instead for 
Did you mean: 

DirectModel symbol NX in Teamcenter ?

Genius
Genius

Hello

DirectModel NX symbol in Teamcenter ?

What is this ? I imported similar 3D-Parts from NX 9 to TC and now:

  • 1st xxx59 does not have a DirectModel.
  • but the 2nd xxx60 has a DirectModel.

What does DirectModel mean and should it be also in the 1st part ?

  • How to input DirectModel to it if it should be in there ?

 

directmodel 5235.jpg

2 REPLIES

Re: DirectModel symbol NX in Teamcenter ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @12131444,

 

The Direct model, is most likely a JT file of the NX part. This is so you can use it i.e. in TCVis. To quickly show a 3D preview.

 

If you turn on, "Save JT data" in you save optoins, you can choose to create the JT or not.

 

If you need it, really depends on your needs. Technically you do not need it Smiley Happy

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: DirectModel symbol NX in Teamcenter ?

Siemens Phenom Siemens Phenom
Siemens Phenom

After setting the option 'Save JT Data', your part must contain 3D solid geometry then only JT dataset will be created in Teamcenter upon saving the part in NX.

 

Refer the following documentation links for more information.

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:index_nxtojt:xid654738:xid641838

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:index_nxtojt:xid654738:xid641579

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New