Cancel
Showing results for 
Search instead for 
Did you mean: 

Display Part with Sketch in Draft

Experimenter
Experimenter

i made some sketch in part, the sketch is in front view

 

in the drafting mode, i want to show those sketch on the projected view, how to do that?

 

thank you Smiley Happy

6 REPLIES 6

Re: Display Part with Sketch in Draft

Experimenter
Experimenter

sorry forgot to mention:

 

it's NX 8.5

Re: Display Part with Sketch in Draft

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you creating a 'Master Model' Drawing where the Drawing file and the Model File are different part files?  If so, is the Sketch in the Model file?  Or are you creating a Sketch in one of the Drawing views?

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Display Part with Sketch in Draft

Experimenter
Experimenter

the model file and the drawing file is linked.

 

i created some simple sketch in the model and want them to show up in a projection view in drafting mode. so whenever i make some changes to those sketch in the model, i want those sketches can update themselves when i click the "Update" in the drafting mode

Re: Display Part with Sketch in Draft

Siemens Phenom Siemens Phenom
Siemens Phenom

You will have to make sure that the Sketch is part of the 'Model' Reference Set.  This is not done automatically so you will need to manually add the sketch to the Reference Set by going to the...

 

Format -> Reference Sets...

 

...and selecting the 'Model' Reference Set in the list and then selecting the Sketch.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Display Part with Sketch in Draft

Experimenter
Experimenter

that works great, thanks for your help.

 

it's a different routine from Solidedge but thanksful, NX let me do this thing. Smiley Happy

Re: Display Part with Sketch in Draft

Siemens Phenom Siemens Phenom
Siemens Phenom

Alternate, we can move sketch to a particular layer and use Layer Visible in View command show/hide that particular layer in required drafting view.