Cancel
Showing results for 
Search instead for 
Did you mean: 

Distorted Graphics with NX 10 and Teamcenter

Valued Contributor
Valued Contributor

I’m seeing the distorted graphics display.

I’ve loaded several different CAD models and all have shown the image weirdness. I attached a screenshot

3 REPLIES 3

Re: Distorted Graphics with NX 10 and Teamcenter

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Since you're seeing your problem with multiple parts, my guess would be that you have a problem with your graphics device driver.  Make sure you have the certified driver installed for your hardware configuration.


Regards, Ben

Re: Distorted Graphics with NX 10 and Teamcenter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I concur.

1) Make sure you have supported hardware (in particular the graphics card) - I have seen similar behavior on "business class" (as opposed  to "engineering class") laptops

2) Make sure you driver is up to date.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Distorted Graphics with NX 10 and Teamcenter

Valued Contributor
Valued Contributor

Thanks fellas, I updated the driver and everythiing looks good. Thanks!