Cancel
Showing results for 
Search instead for 
Did you mean: 

Dock Layer Settings

Pioneer
Pioneer

Hi,

 

I was wondering if there was a way to dock the Layer Settings in NX.
I often work with more bodies or surfaces inside one model. Instead of hiding/unhiding stuff - I assign them to layers. It bugs me I have to turn on the layer settings each time I want to turn a layer on or off.

 

Could I dock the layer settings menu somewhere?
Is there a better way to handle this?

Thanks!

6 REPLIES 6

Re: Dock Layer Settings

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes..You can create a custom tab and add the commands that you use frequently.

 

CTRL+1, Click on + sign and provide the name to the new tab, I had used as 'My Tool'

 

Tool.PNG

 

Tool_1.PNG

 

 

 

 

Re: Dock Layer Settings

Pioneer
Pioneer

Thanks for your answer, but I have that.

I want to have it always open. Smiley Happy

Re: Dock Layer Settings

Siemens Genius Siemens Genius
Siemens Genius

There is no way to dock the Layer Settings dialog and have it permanently open whilst running other comamnds.  You can use the accelerator Ctrl+L to quickly start the Layer Settings command when you need it.

 

Hope that helps a little!

Re: Dock Layer Settings

Gears Phenom Gears Phenom
Gears Phenom

You could record a journal to turn on/off each layer you want to control and assign each of these to toolbar buttons.

However, its a bit cumbersome, especially if you want to control a lot of the layers this way.

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Lenovo ThinkPad W540, Win7, 16GB. Developing in: Java | C | KF
Production: [NX8.5.3.3 MP11 64bit] Testing: [NX12.0.2 MP1]

Re: Dock Layer Settings

Siemens Phenom Siemens Phenom
Siemens Phenom

Even thought you cannot leave it turned on, the hot key CTRL-L is avaialbe as well as adding it the ribbon bar. There is one other option to get to command you need all the time, just add them to your MB3 View Popup. In this example I put it at the top of the list. This way you can quickly get to the menu and minimize mouse travel. On my view popup I add the Measure Distance command as well.

 

MB3Menu.pngMB3 View Menu Customized 

 

Scott

Re: Dock Layer Settings

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Or add it to a border bar (left/right/top/bottom)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled