Cancel
Showing results for 
Search instead for 
Did you mean: 

Does 'TC_NX_Database_Attributes_For_Load' option needs an attribute mapping in TC item&dataset?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I did create an attribute using the attribute template. And then, use TC_NX_Database_Attributes_For_Load in TC option.

However, attribute was not displayed in attributes list of itemtype & dataset.

I think... if it can be possible, I have to apply attribute mapping in itemtype & dataset.

Is it right?

 

Frankly, I'd like to know why I need the 'TC_NX_Database_Attributes_For_Load' option. 
Help Documents's description is too short. Smiley Sad

 

http://localhost:8181/tdoc/nx/10/nx_help/#uid:xid461526

 

 

Please more information.Smiley Wink