03-09-2018 05:55 AM
Hi,
I imported a STL with two Bodies and try to do an Edge-Blend or Face-Blend but cannot do this. The edge and faces are not selectable. Does someone know if this is possible and, if yes, what I need to do?
Thanks,
Martin
03-09-2018 08:10 AM
03-09-2018 10:08 AM
In NX 12 you can use the command called Create Transition to add "edge" treatments to a Convergent body. As state above there are no real edges on the part it is only facets.
Scott
11-13-2018 09:16 AM
Hello Scott,
So that means in NX 11 one cannot blend the sharp edges of a convergent/facet body since this Create Transition command is only available in NX 12?
Jericho
11-13-2018 09:56 AM
11-13-2018 09:58 AM
Yes that is correct, the add transition command for convergent bodies was added in NX 12.
Also check out this video around the 7:00 mark.
Or this one around the 3:00 mark. This one has some great commands to work with Convergent Bodies.
Scott
11-13-2018 11:00 AM