Cancel
Showing results for 
Search instead for 
Did you mean: 

Double information on balloon

Phenom
Phenom

Hi,

it's possible to have the part number and the callout in the balloon ?

ugraf_2018-05-22_12-00-18.png

Thank you...

Using NX1867
RuleDesigner PDM

6 REPLIES 6

Re: Double information on balloon

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

if you created the Balloons manually then you can link the lower value to a callout.

When you see the dialog go to the edit text of the lower text.

Change category to relationships ->use Insert Object attribute

 

Here you can select the component where you want to use the callout from.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions
Highlighted

Re: Double information on balloon

Phenom
Phenom

Hi @ruud_vandenbrand,

balloon are added automatically.

Callout and part name is an option available on part list setting, but I'm not able to set Callout and 'custom attribute'.

Thank you...

Using NX1867
RuleDesigner PDM

Re: Double information on balloon

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @cubalibre00,

Parts List Settings, try this

Symbol - Divided Square

Main Symbol Text - Custom

Custom Text - "<T<W$=@$PART_NAME>!$~C>"

You may need to adjust balloon size accordingly.

Re: Double information on balloon

Phenom
Phenom

Hi @GaneshKadole,

thank you for the support.

I tried to use a custom attribute , because there are part numbers different to file name.

For example we have some part numbers with this syntax '4-100100/00' but the file name is '4-100100-00' because Windows doesn't accept special characters. So we use a custom attribute for the part number.

Your string <T<W$=@$PART_NAME>!$~C> works fine, but if I replace PART_NAME with our custom attribute like this <T<W$=@$Codice>!$~C>, it doesn't work.

Again, it's possible to position texts centered and set a different height for the 'Divided Square' ?iexplore_2018-05-16_15-52-41.png

Thank you...

Using NX1867
RuleDesigner PDM

Re: Double information on balloon

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @cubalibre00,

 

Your string <T<W$=@$PART_NAME>!$~C> works fine, but if I replace PART_NAME with our custom attribute like this <T<W$=@$Codice>!$~C>, it doesn't work. 

Remove the highlighted "$" preceeding the Codice attribute.

 

Again, it's possible to position texts centered and set a different height for the 'Divided Square'

Lettering Preferences

For balloon symbols, all text created within the symbol is center justified regardless of the Alignment Position setting.

 

ER 6023246 - Allow alignment/justification of text in an ID Symbol/Balloon

 

Regards, Ben

Re: Double information on balloon

Phenom
Phenom

@BenBroad wrote:

Hi @cubalibre00,

 

Your string <T<W$=@$PART_NAME>!$~C> works fine, but if I replace PART_NAME with our custom attribute like this <T<W$=@$Codice>!$~C>, it doesn't work. 

Remove the highlighted "$" preceeding the Codice attribute.

 

Again, it's possible to position texts centered and set a different height for the 'Divided Square'

Lettering Preferences

For balloon symbols, all text created within the symbol is center justified regardless of the Alignment Position setting.

 

ER 6023246 - Allow alignment/justification of text in an ID Symbol/Balloon

 

Regards, Ben


Hi @BenBroad,

thank you for your rapid response and solution.

I verified for lettering preferences and on NX 11.0.2 for Balloon, changing preferences did not reflect.

Then the ER is for this case.

Thank you...

Using NX1867
RuleDesigner PDM