Cancel
Showing results for 
Search instead for 
Did you mean: 

Drafting_Feature_Edit

Builder
Builder

Hello NX Guys,

 

 I wanna ask crazy question ,

 

1.Is that possible to change Feature parameters in Drafting Module without PMI InheritSmiley Very Happy

 

 

2. In Drating module Feature parameter command , i cant insert dimension of features like extrude, groove etc detail,

Is there option to inherit dimension like  extrude ,groove  etc dim. in dimension (without PMI Inherit., actually i wanna insert direct dimension to drafting view)Smiley Wink

 

 

Have anybody idea for this 

 

 

 

 

 

 

 

Warm Regards
Thomas Roman
Machine Designer
8 REPLIES

Re: Drafting_Feature_Edit

Phenom
Phenom

@Thomas_Roman wrote:

Hello NX Guys,

 I wanna ask crazy question ,

1.Is that possible to change Feature parameters in Drafting Module without PMI InheritSmiley Very Happy

2. In Drating module Feature parameter command , i cant insert dimension of features like extrude, groove etc detail,

Is there option to inherit dimension like  extrude ,groove  etc dim. in dimension (without PMI Inherit., actually i wanna insert direct dimension to drafting view)Smiley Wink

Have anybody idea for this  


No.  I would like PMI for all :-).

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

Re: Drafting_Feature_Edit

Builder
Builder

Hello bro,

 

In PTC Creo my friend told me that

 

you can directly add the extrude, revolve, etc feature dimensions in drafting

 

i think IN NX should have to solution for this 

 

Actually i dont want to give dimension more times,,..................

Warm Regards
Thomas Roman
Machine Designer

Re: Drafting_Feature_Edit

Phenom
Phenom

@Thomas_Roman wrote:

Hello bro,

 

In PTC Creo my friend told me that

 

you can directly add the extrude, revolve, etc feature dimensions in drafting

 

i think IN NX should have to solution for this 

 

Actually i dont want to give dimension more times,,..................


Without PMI license no.

Please refere to the other topic..

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

Re: Drafting_Feature_Edit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor


Without PMI license no.

Please refere to the other topic..


Actually, you can; it's just not recommended. See my first post in the linked thread and BenBroad's reply to it.

Re: Drafting_Feature_Edit

Phenom
Phenom

@cowski1 wrote:


Without PMI license no.

Please refere to the other topic..


Actually, you can; it's just not recommended. See my first post in the linked thread and BenBroad's reply to it.


Sorry, but there are lot of limitations to use. I'm not feel to suggest.

Thank you...

Using NX11 and NX1847
RuleDesigner PDM

Re: Drafting_Feature_Edit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not suggesting it either; but to say it is impossible without PMI is misleading.

Re: Drafting_Feature_Edit

Builder
Builder

Hello Guys ,

 

I got it that we can't direct insert dimension via features

 

but we can change dimension via Expression in drafting module,

 

,but is there any option to add expression dimension in drafting view via any command!!!!!!!!!!

 

 

anybody have idea

 

 

 

 

Warm Regards
Thomas Roman
Machine Designer

Re: Drafting_Feature_Edit

Builder
Builder
any option to inherit dimension of expression in drafting view,,


Best Regards,
Thomas_Roman
Warm Regards
Thomas Roman
Machine Designer