Cancel
Showing results for 
Search instead for 
Did you mean: 

Drafting Symbols

Experimenter
Experimenter

I need to create a great then and equal too, i was wondering if there what a symbol for that and if so how would i type it into a note.

 

Also I was wondering if there was a cheat sheet showing all the symbols with the short cuts for drafting

5 REPLIES

Re: Drafting Symbols

Honored Contributor
Honored Contributor

If you are using a true type font, you can use the Windows utility "character map" to copy & paste any character from the font you are using to your note.

 

Alternatively, you could use a greater than sign and format the note to underline that character. It will end up looking just like a "greater than or equal to" sign and works with any font.

Re: Drafting Symbols

@cowski1 Being curious about it, Can you please guide, How can we map it?

Ganesh Kadole, QA Analyst (PLM), SQS
Testing: NX 11 | NX 12 | TCIN
TC 11.2 | TC Vis 11.3 | AWC 3.2

Re: Drafting Symbols

Honored Contributor
Honored Contributor

I'm not sure what you mean by "how can we map it", but here is a quick rundown on the "character map" utility (assuming you are using a Windows OS):

  1. start menu -> search programs and files -> "character map"
  2. open the character map program, choose the desired font
  3. all of the available characters in that font will be shown in the listbox
  4. selecting a character will show you the keycode to enter it from the keyboard or double clicking it will copy it into the text box; from here you can copy & paste the text into other applications (such as NX).

Re: Drafting Symbols

Esteemed Contributor
Esteemed Contributor

And if you are using a "legacy" NX font (blockfont, etc.)

I have attached a file.

- open the file

- Select everything that is selectable (note the "headers" are on a layer that is visible but not selectable, this is intentional)

-> Style

- change to desired NX font

 

Note this only shows the legacy (ASCII + $ characters) not the full Unicode set (some fonts have Unicode characters)

- You can see what characters map to what symbols (in particular, the "$" characters)

 

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Drafting Symbols

@cowski1: You explained what exactly I want to know.

@Ken_A: Thank you for your comment, It is also useful.

 

You guys are great! Smiley Happy 

Ganesh Kadole, QA Analyst (PLM), SQS
Testing: NX 11 | NX 12 | TCIN
TC 11.2 | TC Vis 11.3 | AWC 3.2