Cancel
Showing results for 
Search instead for 
Did you mean: 

Drafting, "Feature Parameters"

Gears Phenom Gears Phenom
Gears Phenom

I noticed that Insert, Dimension, Feature Parameters is currently hidden, NX9.

 

Is it just my role, or is "Feature Parameters" on the way out?  If on the way out, what replaces it, in regards to dimensioning external threaded features?

 

Thanks,

Dave

 

 

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
2 REPLIES

Re: Drafting, "Feature Parameters"

Siemens Phenom Siemens Phenom
Siemens Phenom

I suspect that it will remain until at least after we start to support annotation callouts for Male threads on both the face of a Drawing and as PMI annotations.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Drafting, "Feature Parameters"

Valued Contributor
Valued Contributor

If on the way out, why????

Why get rid of something that works????

Will the 'new' feature still recognize lagacy files????

We go back to NX3 for legacy, and 'new' features usually cause issues on these legacy files.

Hope serious consideration is given to this....