Cancel
Showing results for 
Search instead for 
Did you mean: 

Drafting view restors previus screen view when press cancel key problem

Drafting view restors previus screen view when press cancel key in a command dialog

or when we finish a dimension

7 REPLIES 7

Re: Drafting view restors previus view when press cancel key problem

I want to keep fix the window not fit window every time

Re: Drafting view restors previus view when press cancel key problem

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @Tooling-Design,

 

I think I understand your question now.   It sounds like you invoke a command in drafting, zoom into an area on the drawing and then cancel the command and NX zooms out to show the entire sheet.

 

If this is the behavior you're seeing, then we already have an existing Enhancement Request (ER) asking that the drawing remain zoomed in when the command is cancelled: ER 5904125.  You can open an IR with GTAC and ask that you're added to the ER so you are notified regarding any updates to the ER.

 

Regards, Ben

Re: Drafting view restors previus view when press cancel key problem

Yes that is the Idea  It is terrible when the software zooms out to show the entire sheet

 

Do I have to send a report?

I don't understand GTAC and ER

 

Thank you very much

Re: Drafting view restors previus view when press cancel key problem

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @Tooling-Design,

 

GTAC - Global Technical Access Center (support for PLM Solutions' products).

ER - Enhancement Request

 

To submit an ER, open a new Incident Report (IR) with your local GTAC office explaining that you would like to submit a new enhancement to the product.  They will have you complete a template to describe why the ER is required and then close your IR as an ER.  For existing ER's, such as the one above, simply inform the support engineer that you would like to be added to the existing ER and give them then ER number.  They will take care of the rest.

 

Regards, Ben

Re: Drafting view restors previus view when press cancel key problem

Ok I will send a report
thank you Ben

Re: Drafting view restors previus view when press cancel key problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note many dialogs behave similarly, e.g. if you change the layer settings while IN the dialog, they are not retained if you cancel.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Drafting view restors previus view when press cancel key problem

gtac.PNG