Cancel
Showing results for 
Search instead for 
Did you mean: 

Drawing Component - Replace Component option back in NX 11

Genius
Genius

I know in the past it was possible to use "Replace Component" on Drawing Components, and then the option was removed, because it was not supported from Siemens (or at least this is the way I remember it).

 

Today we were looking something in NX 11, and we found that "Replace Component" was available again for Drawing Components.

 

Does anybody know anything about this option beeing available again for users?

 

Thank you

6 REPLIES 6

Re: Drawing Component - Replace Component option back in NX 11

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
I just tested NX11.0.1 and I do not see the option. The NX11.0.1 documentation continues to state "... you cannot use the Replace Component command on a drafting component".
Which version of NX11 are you using, and can you post a screenshot of the popup menu showing "Replace Component"?

Regards, Ben

Re: Drawing Component - Replace Component option back in NX 11

Genius
Genius

this is NX 11 for Daimler.  I think it's NX 11.0.0 plus a specific patch for them (D3)

Re: Drawing Component - Replace Component option back in NX 11

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Not seeing it in NX11.0.0. D3. Maybe it's something unique to the Daimler environment, as I only have access to the build, not the environment files.

Re: Drawing Component - Replace Component option back in NX 11

Siemens Phenom Siemens Phenom
Siemens Phenom

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Replace-component-for-drafting-refer...

 

This topic discussion explains all about 'Replace Component' option for Drawing/Drafting component. Prior to NX 9 it was available.

 

Re: Drawing Component - Replace Component option back in NX 11

Pioneer
Pioneer

I still don't see a way to replace a drafting component in NX11.0.2.7 mp5.

We have alot of drawings with multiple components, some modeling and some drafting components.

 

Please tell me how to replace a drafting component in a drawing file.

drafting_comp.jpg

Victor Cohen Engineering manager American Tool & Mold NX11.0.2.7 MP5 Windows10 Nvidia Quadro P5000

Re: Drawing Component - Replace Component option back in NX 11

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

There is a workaround that we were able to find.
If you add the same component in modelling and then replace the model component (making sure replace all occurences is turned on), the drafting component will be replaced as well.

The video below should explain how that's done.

 

(view in My Videos)

Anthony Galante
Senior Support Engineer
PhoenxPLM