Cancel
Showing results for 
Search instead for 
Did you mean: 

Drawing Sheet Suppresion

Siemens Phenom Siemens Phenom
Siemens Phenom

Like in Modeling application, we can suppress the individual features. Is it possible to suppress the individual drawing sheet in drafting?

 

I am verifying the check mate checkers (Customized). Each time I need to create a new drawing sheet with fail conditions. So finding way to avoid it if there is option to suppress the drawing sheet or any workaround. 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

4 REPLIES 4

Re: Drawing Sheet Suppresion

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"Like in Modeling application, we can suppress the individual features. Is it possible to suppress the individual drawing sheet in drafting?"

 

No.

Re: Drawing Sheet Suppresion

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

that's clear Smiley Happy


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Drawing Sheet Suppresion

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I know it wasn't the desired answer... Smiley Frustrated

Re: Drawing Sheet Suppresion

Genius
Genius

I placed an ER for setting a drawing sheet as not printable and/or not countable for total sheet count, and other for add to print/export menu the option to print all sheets without need to manually select all of them. I think the purpose is very similar of what you intend to do. I think any way of doing that would be very useful.