Cancel
Showing results for 
Search instead for 
Did you mean: 

Drawing arrangement: 1,2,3,n,.. How functions ?

Genius
Genius

Hello (NX 9)

Someone has made Arrangements 1,2 in to the drawing: how do they function and what can I do with them ?

 

arrangements.jpg

1 REPLY

Re: Drawing arrangement: 1,2,3,n,.. How functions ?

Experimenter
Experimenter

arrangement are made in assemblies and can be placed on a drawing.

 

With assembly arrangements you can controle different positions of one or more components by using assembly constrains and component suppressions.

When you have a assembly you can start to create some arrangements as many as you needed to display the assembly with different options/positions

example:

back

forward

middle

only left piston

only right piston.

 

now you can make a constrain arrangement specific.

after the go to the new constrain (angle or distance) rmb and click on edit in arrangement

here you can choose with angle you want for which arrangement.

 

for the suppression you can select a component or sub assembly then rmb-> suppresions.

her you can select in which arrangement you want to suppres that component/subassembly

 

below you will find some examples.

 

arrangement_overview.JPG