Cancel
Showing results for 
Search instead for 
Did you mean: 

Drawing lines are same size as dimension lines ?

Genius
Genius

Hello

Drawing lines are same size as dimension lines ?

  • Does these lines look like NX9's default line settings ?

 

sheet2244.jpg

8 REPLIES 8

Re: Drawing lines are same size as dimension lines ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

I guess no.....can you please check the drafting standard being used (ISO???)

Best Regards

Kapil Sharma

Re: Drawing lines are same size as dimension lines ?

Siemens Phenom Siemens Phenom
Siemens Phenom

one probable setting may be this...if you see same thickness for drafting and dimensions line.

drafting.jpg

 

Best Regards

Kapil

Re: Drawing lines are same size as dimension lines ?

Genius
Genius

I opened one drafting and it says 0.18mm ?

  •  Where to see "Drafting Standard" ?

sffsf.jpg

Re: Drawing lines are same size as dimension lines ?

Siemens Phenom Siemens Phenom
Siemens Phenom

ok...it is the default setting then....

You  can check the drafting standard from...FILE/UTILITIES/CUSTOMER DEFAULTS/DRAFTING /GENERAL /STANDARD...by default it is ISO(shipped).

Regards

Kapil

Re: Drawing lines are same size as dimension lines ?

Siemens Phenom Siemens Phenom
Siemens Phenom

i forgot to mention one thing...it seems to be a flat pattern drawing (anything related to one of your older threads?)  . did you change the flat pattern drawing settings (if i am not wrong Dave suggested some settings in his reply)

Regards

Kapil

Re: Drawing lines are same size as dimension lines ?

Siemens Phenom Siemens Phenom
Siemens Phenom

I would recommend setting up your environment according to your company drafting standards.

  1. Set your standards using Customer Defaults-->Drafting-->General/Setup-->Standard-->...
    Use one of the OOTB standards or customize to suit your needs using 'Customize Standard'
    For example:
    2017-04-19 10_50_27-NX 12.0.0.16.jpg
  2. Set the flat pattern defaults using Customer defaults-->Sheet Metal-->Flat Pattern-->Curves
  3. Create drafting templates using these settings.
    (follow the help documentation to do this)

 

Once setup correctly, each and every drawing will be created to your requirements.

Re: Drawing lines are same size as dimension lines ?

Genius
Genius

Where are the .PDF conversion line thickness values ?

  • PDF turns lines thin again.

fdsfd.jpg

Re: Drawing lines are same size as dimension lines ?

Siemens Phenom Siemens Phenom
Siemens Phenom

How are you creating the PDF?  Ensure your chosen method is setup correctly.  I have tried all three of the methods shown below and can see a diffierence in line width between outline and dimension

 

File-->Export-->PDF (do you have single width set here? Try Standard Widths)

2017-04-19 13_28_26-Export PDF.jpg

File-->Print...

2017-04-19 13_30_14-NX 12.0.0.16 - Drafting.jpg

File-->Plot

2017-04-19 13_31_16-Plot.jpg