Cancel
Showing results for 
Search instead for 
Did you mean: 

Drawing no attribute display while exporting PDF from NX?

During exporting PDF drawing from NX: Instead of displaying default DTM ID, I want the drawing no attribute to be automtically displayed. (refer the yellow highlighted area in attachment).

 

Cheers,
Karthick.
4 REPLIES 4

Re: Drawing no attribute display while exporting PDF from NX?

Siemens Phenom Siemens Phenom
Siemens Phenom

@Karthick_Raja 

Does "0000354804_002" indicates the drawing number ?

Re: Drawing no attribute display while exporting PDF from NX?

@GaneshKadole 

No, it was the default DTM ID of that item created by TC. I have a separate drawing no for that item.

Cheers,
Karthick.

Re: Drawing no attribute display while exporting PDF from NX?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Karthick_Raja 

You need to enter that attribute name manually. I see there are some ER's present already requesting similar functionality, including one to use attribute (in the default dataset name while exporting PDF) as you have asked.

Re: Drawing no attribute display while exporting PDF from NX?

@GaneshKadole 

Yes. While entering the attribute name manually, sometimes it is possible for mistyping.

To overcome this, better we have the option for selecting which type of attribute to be displayed while exporting PDF.

Cheers,
Karthick.